Other Parts Discussed in Thread: TPS92518
Hi Team,
Customer is searching for a LED driver for automotive and they are interested with TPS92518. Below is the inquiry.
1. Can this driver handle different currents? so is it possible to adjust the current settings via SPI?
> based from the discussion in this link : https://e2e.ti.com/support/power-management/f/power-management-forum/752536/tps92518-output-current-problem , this driver can handle different currents via SPI.
2. The input voltage is between 20 and 40V. The output current is 200mA to 3.5A. Is it possible to reach this values with only one single inductor with around 120uH?
Thank you in advance.
Regards,
Maynard