Other Parts Discussed in Thread: LM5022
Hello team,
My customer would like to design isolated DC-DC with LM25184.
The following is the specification.
Vin 20-26 V
Vout 15V
Iout 2~3A
Isolation is needed at output.
The customer tried to do webench simulation, however " Design cannot be created." was shown as the result of webench.
Is the power consumption too large for LM25184?
If yes, what do you recommend in TI devices?
Your advice would be so appreciated.
Best Regards,
Akihisa Tamazaki