Other Parts Discussed in Thread: TPS2H000-Q1, , HSS-MOTHERBOARDEVM
Hi,
In the recommended operating conditions section of datasheet
Maximum extended supply voltage is given as 28V.
There is a note given for the extended supply voltage is that 'device would function within extended operating range, however some parametric values might not apply'
Can you please evaluate more on the note. On my board the IC is running on 12V or 24V. When 12V supply a maximum of 110mA can be drawn at the output of the IC.
When a 24V supply is given, a maximum of 40mA can be drawn at the output of the IC.
When given 24V supply there is 4V drop observed at JP1 on no load condition. When i draw 25mA on that line the voltage drops to 5mA. Can you tell me reason for that behaviour?
Shown schematic section below
Regards,
Sahil