Hi team
I'm trying to generate -5 V from a 5 V supply using the LM2611AMF CUK converter, but I get very low voltage on the output and a large current draw (on the order of 400 mA) when I try to hook-up the device. Right now I'm only testing it from a power supply. I've attached my circuit schematic and layout. I realize that some of lines route over the switching paths, but the layout is on a 4 layer circuit board, which I was hoping would provide enough shielding. I've also try removing U10, but that does not fix the issue. I guess it could also be a soldering/board assembly issue, though I think this is unlikely as I've had this issue on multiple boards and they were assembled by a commercial vendor.
Is the an obvious issue with my layout for example that could cause this issue?
Any suggestions for things that I could try? Thanks!LM6211 Layout (1).pdf