Other Parts Discussed in Thread: PMP9253
Hi Sir
I used the LM5022 be the flyback converter.
Attached is my circuit.
When I saw the TI document, the D4 and D5 are DNP.
Here is the circuit which cut from PMP9253.
If there is no diode and when MOS is turn off, where the current flows?
So I added one resistor, one capacitor and a diode.
Also could you help me to check the whole circuit?
The input voltage is from 18~52V, and output V/A is 5V/4A.
BR
Charge