This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL7660: Problem with generating -5V using TL7660

Part Number: TL7660

Hello, I am trying to generate -5V using TL7660. I am using 2 capacitors (c1 and c2) 10uF tantalum type same as the datasheet suggested (C1 positive is with pin 2 and C2 positive is grounded). But when I am providing +5V or +3.3V in Vcc the out is always +0.25V.  I can't figure out why its happening. Can someone suggest how the circuit should be for TL7660?

Thanks in advance.

Shamsul