Hi, BQ24179 support team
The below is system requirement.
- Input Voltage = 20V
- Charging voltage = 13.65V
- Charging current = 2.1A (1.2CA)
- Cell structure = 3cells
- Cell voltage range = 3.0 - 4.55V/cell
Do you think that BQ24179 can support the above application?
As far as I see the Figure.7-3, BQ24179 looks like to be able to support up to 64W at least.
Thanks
Tamio