Hi, it's mentioned in page64 that "Capacitors should not be connected from the pins to VSS" while in page75 it's told "Optional 0.1-uF filter capacitors can be added at each sense input pin to ground". What's the real story? If 0.1uF is increased, say 1uF, what will happen then?
BTW, could two-stage RC filter be placed between SRP and SRN in order to further filter out the ripple across the shunt resistor when pack is charged? Any restriction about the low-pass filter? Thanks.