Hi,
My question is:
1) When does Vosns turn on if the output voltage is generating? Does FB(pin7 of TPS61096A) samples all the time during the opening and holding time of Vosns?
2) Is the opening and holding time of Vosns fixed or variable( I actually test that the opening and holding time of Vosns is about 10us)?What is the relationship between the opening and holding time of Vosns and output load( for example,if the output load is heavy,the opening and holding time of Vosns will increase or decrease?If the output load is light,the opening and holding time of Vosns will increase or decrease?)
Thanks a lot!