Other Parts Discussed in Thread: CSD18563Q5A
I used LM5117 to design two outputs, input voltage 25~40V, output1 is 12V/10A, output2 is 22V/4A, output 1 is ok, but output2 is less than 22V without load and is ok with load. They're on the same circuit board and the same frequency.