Hi
I design as below with LM51501-Q1.
-Input: 4.5~12V
-output: 11.5V 8A
1. Is it possible to bypass the input voltage above 11.5v without boost?
2.Is it possible up to 8A?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I design as below with LM51501-Q1.
-Input: 4.5~12V
-output: 11.5V 8A
1. Is it possible to bypass the input voltage above 11.5v without boost?
2.Is it possible up to 8A?
Thanks
Hi David,
1) In boost topology, you have a high-side path from input to output. So if input voltage is higher than output regulation target, you can bypass.
2) High side path consists of inductor and diode, so you would make sure components can handle the current ratings.
Thanks,
Richard