This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25970: TS ADC range in percentage meaning?

Part Number: BQ25970

BQ25970 manual states

TS ADC reading
Type : R
POR: 0% (0h)
Range : 0%-99.9023%
Fixed Offset : 0%
Bit Step Size : 0.0976563%

What does the percentage mean? What is 0% and what is 100% in Celsius?