Hello,
I am using the LMR33620ADDA to provide 9.5V at 1.5A from an input supply of 10.5V to 18V. I've used Webench to create the design. Webench is asking for 5 15UF output capacitors with an "effective" capacitance of 16UF. Won't 5 15 UF capacitors give a much higher effective capacitance than 16UF? I can see using perhaps 2 capacitors . . . but, why 5? Just want to double check before committing the design to a prototype.
Thanks for your help,
Max