This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24041: Placing BQ24041 instead BQ24040

Part Number: BQ24041
Other Parts Discussed in Thread: BQ24040, , BQ24072

Hi.

For a project we are considering change the BQ24040 and place the BQ24041. 

In the project we have we need to have an output with and without a cell connected to the output. And the output current is almost  1 A.

We have the following:

To place the BQ24041 and have same behavior we reviewed the datasheet and we will remove the R201 connected to Pre-term in BQ24040 and change the R202 connected to TS in BQ24040 to a 0 Ohms resistor to enable always the BQ24041.

Could you tell me if the analysis is ok, that we get same behavior only doing that?, in case not, could you explain me the difference or what we need to have same behavior?

Regards