Other Parts Discussed in Thread: SN6501,
Hello all
I have the following circuit:

-OFFV_L is -10VDC. The switching voltage is -10VDC/+16.5V
I want to use the circuit with frequencies down to 0Hz so that one MOSFET is continuously turned on. Of courcs this is not possible with the bootstrap circuit.
I thought and tried to suply the BOOT pin with external +22VDC but it did not work (TPS28225DRB gets damaged).
- Is it even possible to use the TPS28225DRB in a static condition?
- If so, what is the problem with my suggested solution?
- How can I change the circuit to achieve the required function?
Thanks for your help.
Best regards