Dear
I would like to ask you about the use of bq25792.
Can bq25792 only add PD controller to realize fast charging?
With the addition of PD controller, is the maximum charging current of one battery cell also 2A?
Does bq25792 have a way to select different charging currents through hardware settings without adding PD controller? If I use battery in an urgent way, I can choose a high current gear. If I don't use it, I can
choose to charge slowly. Can I do this in a way?
Thank you very much!