This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43061: TPS43061 as s TPS43060 substitute

Part Number: TPS43061
Other Parts Discussed in Thread: TPS43060, , CSD18543Q3A

Hi,

I designed a circuit for the TPS43060 using webench to create a 36V 1A DC supply from a 6 to 8V DC input. The first articles worked fine, but TPS43060 is now out of stock.

When I replaced it with TPS43061, removed the bootstrap diode and replaced the 2Ohm resistor with a 0Ohm resistor, I started having overheating of QL (CSD18543Q3A).

I understand all other parameters (switching freq, compensation circuit) could stay the same.

Thanks,

Ashraf