Hello,
I am aware that the main difference with the TPS53622A is the added ability to program the OVP threshold to 200mV or 400mV. From that, I am confident the A-part would work just fine in a system designed with the non-A-part.
My question is: Would the programming file (.csv) from a TPS53622 work on the TPS53622A? The first line in our programming file suggests it would not work:
Comment,Verifying IC_DEVICE_ID is 0x22 (TPS53622)
BlockRead,0x60,0xAD,0x0122
If it does not work, is there a template file for the TPS53622A? I tried to create one with the GUI (Version 7.3.1) but it was not under the supported device list.
Thanks!
Yale