Other Parts Discussed in Thread: TPS2113
Hi,
We are looking to use TPS2113 to Mux two 5V supplies. One from a 5V regulator 2A and one from 5VUSB. I tried to design the circuit such that, IN1 (5V external) is prioritized and switches over to IN2 (5VUSB) when IN1 falls below 4V or VSNS < 0.8V. Also, we designed it to use the STAT pin such that the LED will turn on when the STAT pin is Hi-Z state (5V output comes from 5V USB).
I am attaching the sample schematic here. Will this work according to how I mentioned it above?
Thank you and suggestions are welcome too.