Dear Support team,
I want to use EQ24650 in my design. I have some queries regarding that please guide me.
1) In my application, I want 3 terminals, 1 is for solar panels, 2nd is for battery charging and 3rd is for connect load. so when the battery is charging at the same time I get regulated output.
2)is there in current limiting for the load which I have connected. one is battery and another is my system, so want to know the current limit for the system.
3)it is possible to set the cutoff voltage? that requirement is because if there is no set of cutoff then my battery is a drain to threshold volt which is 2.11Vand when start charging through solar it will take time. if there is a provision I will set the cutoff voltage after that voltage my battery does not give voltage so the load does not get the output. so charging time is minimize and the battery will not drain completely.
Please guide.
Thanks