This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82140: tps82140

Part Number: TPS82140


Hello, 

When the datasheet of this IC is looked, the input range is 3V-17V whereas the output voltage 0,9V-6V and the output voltage can be adjusted with resistor placed in pin of the IC. There is a question about this conversion. this IC is buck or boost converter? So, does 5V can be produced during either 3V input is supplied or 7V is supplied? I think there is no information against this idea instead of the fact that "step-down converter" is written. IN other words, does VFB(voltage of the feedback pins of IC)  give a constant value as the input voltage range is 3V-17V?