Other Parts Discussed in Thread: LP2954, TPS7B86-Q1, LM5069
Dear Power Management Team,
I have some questions about the output Isolation feature et some charateristics of the LP2954 :
- Is the output stage a bipolar transistor as shown in the block diagram of the datasheet ?
- What is the value of the Reverse Output Current ? (e.g. with the input grounded and the output set at a specific voltage)
- What is the maximum voltage that could be applied at the ouput when the input is grounded ? Absolute maximum rating of the Output pin voltage does not appear in the datasheet.
- Is there a reverse current protection when the ouput is connected to an active voltage source and when the input is set to a specific inferior voltage ? e.g. active voltage source at output=20V and input=15V.
For information, I plan to use two LP2954AIM (adjustable) with their outputs tied together to act as an ‘OR’ function.
BR,
Guillaume