This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560430: 5V then to output to 3.3V LDO

Part Number: TPS560430
Other Parts Discussed in Thread: TPS560200-Q1

Dear Sir/Madam

Our PCB requires 5V and 3.3V. Max Vin can be 24V

The 3.3V will be used for all the wifi and uC circuits, max 350mA

The 5V is needed as a pullup on a PWM signal to a fan, max few mA.

I intended to use this device to generate the 5V, then use a simple SOT23 LDO to generate 3.3V. Would this be the best way or can you offer any better suggestions?

Can we also use following inductor with this device?

Murata LQH43PN100M26L