Other Parts Discussed in Thread: LM5160
Hi Team,
The customer is using the LM5160-Q1 for the electric compressor inverter.
Even if the secondary circuit enters Sleep mode and does not consume electricity, 20 mA is consumed continuously switching the Transformers in the Fly-buck circuit on the primary side.
The customer wants to enable/disable the LM5160 IC using CAN Transceiver with wake-up function.
Q1: Is there any way to enable/disable LM5160 IC using CAN Transceiver with wake-up function?
Q2. If there is another way to enable/disable LM5160 IC, please recommend it.
Delete schematic