This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560200-Q1: Design advice

Part Number: TPS560200-Q1

Hi

I aim to use the TPS560200-Q1 in design to get 3.3V max 400-450mA during peak Wifi TX, otherwise less then 100mA. My Vin will be 12V

This is my design, i have not yet done PCB layout.

I prefer to keep my BOM as universal possible, therefore, would there be any issues using the following components:

10 uF Inductor -> LQH43CN100K03

10uF Capacitor 0805 ->CL21A106KOQNNNG

This is the PCB layout

I await your reply

Thank You