This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: Search TI solution

Part Number: TPS1H100-Q1
Other Parts Discussed in Thread: TPS2HB35-Q1, TPS2HB50-Q1, TPS272C45, TPS2H000-Q1

Hi Team,

Reference TPS1H100BQPWPRQ1
Does TI have 2CH and can be controlled separately
And then sealed in the same IC
Single CH maximum current 3A

Vin:9V~16V

THX

  • Hi Kygo,

    I was searching for the part, and the TPS1H100's HTSSOP (14) package is quite unique. I can fid some replacement part for 2 channels in HTSSOP (16) package that can meet your requirements. The size of the package is the same, but the pins won't be compatible. 

    The parts are: TPS272C45, TPS2HB50-Q1, TPS2HB35-Q1 and TPS2H000-Q1

    Please let me know if you need further help.

    Regards,

    Yichi