Hi Team,
Pls help to review the attach LM5069 schematic. Thanks in advance for your help.
The 24V supply is from a 360W AC-DC converter and the current limit at J803 is 8A, the load capacitance (not shown in the schematic) is 1000uF max. Ambient temperature is 40 degC.
Attached is the LM5069_Design_Calculator tool filled with value base on the design requirements fyr. We notice the recommended Timer capacitance is 303nF. We will consider 330nF (the next standard value available), is this ok?
Look forward to your comment from the review. Thanks.
TF_LM5069_Design_Calculator_REV_C.xlsx
Regards,
Don