This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF3425: REF3425IDBVR does not provide 2.5V.

Genius 9880 points
Part Number: REF3425

Hi Team,

We have received inquiry from customer that our IC REF3425IDBVR does not provide 2.5V. 


According to them, the device output always below 2.5V with/without the decoupling which they cannot proceed the evaluation. Below is the output result.



All the purchased REF3425IDBVR has an output of 1.44V for all "DC voltage" with decoupling (Without 1.38V). In both cases it oscillates heavily. The customer suspect that device are dead on arrival
"

Thank you in advance.

Regards,

Maynard