Hi team,
Could you help recommend a module or buck converter IC which height is lower than 1.2mm?
The spec requirement is below.
4.5V~18V in/ 3.3V 0.5A out
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There is a APLed part TPS563211/TPS562211 meets your requirements,4.2-18vin 2A/3A buck in SOT 583 package (height 0.6 mm). RTM is in SEP 21.please check if this schedule okay for you.
If an RTMed device needed, we have a spin part of TPS563201 to 18vin , 4.5-17vin,3A in SOT236 pkg (height 1.1mm).
Also you can try TPS56339 , 4.5V-24vin, 3A in SOT236 pkg.
BR,
Young