Hello E2E,
Is it possible to damage the DRVOUT if ferrite beads are installed on the FET gate?
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ACGUY,
adding ferrite bead on the mosfet Gate pin is commonly used to help reduce the ringing on the VGS. It should also help on the DRVOUT on the controller side.
Please make sure the voltage on the DRVOUT do not over the controller's spec requirement. The controller can be safe if all the voltage on the controller can meet the datasheet requirement.
hope this helps you.
Hi David,
Thank you for reply.
I understood about ferrite on Gate by your comment.
Our customer changed the FET for PFC from R6025ANZ(Rohm) to R6050JNZ(rohm), many UCC2818A were damaged.
The damaged devices has near short between DRVOUT and GND.
I don't think there is a quality issue with the device, but I haven't been able to determine the cause.
Can you guess the cause of this event?
Regards,
ACGUY
Hi ACHUY,
I guess over votlage stress on the DROUT pin let the controller fail.
Please check the votlage especially at transient /start up/ ocp condition to see whether the votlage already over spec.
you can also try to increase the turn on/off resistor to lower the influece from mosfet to controller to see whether any improvement.