Hi TI Team,
We are planning to use TPS65262-2 for generating on-board supplies for different interfaces on our board from 5V input. The requirement and our plan is as below
Buck 1 for 3.3V, 3A supply
Buck 2 for 2.5V, 1A supply
Buck 3 for 1.8V, 1A supply
LDO1 for 1.05V, 350mA Supply
LDO2 for 1.0V, 350mA supply.
Could you please confirm that, we can go ahead in this manner.? Also how to take care in design to achieve this configuration with these outputs.?
Best Regards,
Vyshnav Krishnan