Hi TI team,
I'm testing my first circuit with LMQ61460 and I observe that everythings works fine if Vin is under 21V. My configuration i 5A@5V. I've succesfully tested loads up to 5A at 20V input but when I rise input voltage above 22V IC drops output to 0V. I have no idea what's going on. Please point me what to check. Below is my circuit. Thanks in advance.