Dear team
Customer found out that the output voltage ripple has a subharmonic oscillation on the TPS549D22RVFR.Is it normal? Are there any no stability issues?
As below is detail information :
The output voltage has a subharmonic oscillation and the Fsw ripple frequency is around 350kHz. The subharmonic oscillation is~20kHz at 50% load and ~33kHz at 100% load.
1. Transient from 50% load to 100%load.
2. Waveform of SW and Vo as below, at 50% load=13.44A:
many thanls
Denny