Part Number: UCC28086
Other Parts Discussed in Thread: UCC2806, UCC28083
Hi..
One of my customer want to design isolated boost. Below are the specification.
Input voltage - 12V Lead Acid battery (10V to 14VDC)
Output - 250V DC @ 100mA
At present they have selected UCC28086 for the application.
They need help to define the transformer for push-pull configuration. Pls. help for the same.
They also ordered Coil craft transformer, pls. find attachment.
With the present design, even in no load condition design is taking too much of current & MOSFETs are blasting. For the better current ontrol, they are now using CVCC bench top power supplies, but current gets saturating to 3A (power supply limit) but design is not working.
What could be the reason? according to transformer datasheet, primary inductance is 32uH where webench design is showing way higher than the transformer inductance. Pls. find webench file as well. Although I am not very confident on webench simulation as it was showing error but somehow it came up.WBDesign135.pdf
Need help to resolve the issue. Also need Pushpull design calculator for UCC28086
Mitesh
Mitesh