Other Parts Discussed in Thread: TPS40055
Hi,
There has detected a problem, and you can see the output table for two 5Vout.
Test Conditions:
24Vin, the current varies from 0.5A-10A, 5Vout full load (5A)
1. The 24V current is between 0.5A-3A, 24V Current share: normal, 5V Current share: normal
2. The 24V current is between 3A-8A, 24V Current share: normal, 5V Current share: abnormal (it may be worse than without this circuit)
3. The 24V current is between 8A-10A, 24V Current share: normal, 5V Current share: normal
May I ask why changing the 24V load will affect the 5V Current share