dear
Chip with TI (30304000007101: IC/BQ27010DRKR/ SON10-20P-190W /TI)
When tested at normal temperature (26℃), the temperature shows up to 46℃;This temperature is too high, as shown below:
any advice?thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear
Chip with TI (30304000007101: IC/BQ27010DRKR/ SON10-20P-190W /TI)
When tested at normal temperature (26℃), the temperature shows up to 46℃;This temperature is too high, as shown below:
any advice?thanks in advance
hi Abraham
Is there any detials step to calibrate temperature bq27x10 evaluation software ?thanks a lot
Hi Raymond,
Sorry, this part does not require calibration, you can try to reset the gauge to see if the issue goes away.
Best Regards,
Abraham