• BQPRODUCTION: bqProduction skips srec programming with bq28z610-r1

    Part Number: BQPRODUCTION
    Other Parts Discussed in Thread: BQ28Z610-R1, , BQ28Z610, BQSTUDIO, BQ78350

    Hello,

    i tried to program bq28z610-R1 with bqProduction and connected HPA495.

    1. Select 26_1_01-bq28z610R1.bqz Container, no Calibrationen marked, select…
  • BQ28Z610: Battery pack with Bq28Z610 is being used with BQ24075 power path and has conflicts

    Part Number: BQ28Z610
    Other Parts Discussed in Thread: BQ24075,

    When a Battery pack with Bq28Z610 is being used with BQ24075 power path and the battery pack is completely discharged, the battery pack IC opens the FETS in shutdown, and the BQ24075 does…

  • BQ28Z610-R1: Please introduce FAE

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM

    Hi Team,

    We are developing a battery protect / fuel gauge board for a special battery cell. Because we are chasing high temperature performance, we got a high temperature optimized…

  • BQPRODUCTION: Programming and calibrating of e.g. bq28z610-r1 in production without bqProduction or bqStudio

    Part Number: BQPRODUCTION
    Other Parts Discussed in Thread: EV2400

    Hello together,

    does anyone have experiance with programming and calibrating of TI Battery Managment IC in production? For small quantities there is a tool from TI called bqproduction, but…

  • BQ2970: Series circuit with BQ29703

    Part Number: BQ2970
    Other Parts Discussed in Thread: BQ28Z610-R1, BQ40Z50, BQ4050

    Hi,

    I want to power my device with two LiPo batteries in series and each cell should be protected by using a single BQ29703 circuit. So I have designed the following circuit…

  • BQ40Z80: DSG FET control

    Part Number: BQ40Z80
    Other Parts Discussed in Thread: BQSTUDIO, BQ28Z610-R1, BQ40Z50,

    Hello,

    We are trying to log a discharge/charge cycle to use the GPCPackager tool to obtain a ChemID that closely matches our battery cell(s). We are unable to turn on…

  • BQ28Z610-R1: We cannot change seal key when using Bqstudio 1.3.101 or 1.3.102

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQSTUDIO

    Hello Sir:

    Can you help to check why we use BqStudio 1.3.101 or 1.3.102 cannot change the seal key?

    We can change seal key by using BqStudio 1.3.86.

    Please help to provide recommendations…

  • BQ28Z610: impacts of a battery that exceeds the maximum capacity of a gauge

    Part Number: BQ28Z610

    A next gen design will use a 15000mAh battery (1s4p), we currently use the BQ28z610 but it has a listed maximum of 14000mAh. 

    1. What would happen, if the capacity exceeds the max rated capacity of the gauge? 
    2. How would this impact the…
  • BQ28Z610-R1: Single Cell Configuration values

    Part Number: BQ28Z610-R1

    Hello! 

    From section 7.26 of the BQ28z610-R1 datasheet, it states there is a 3.3k pull down on I2C. Can you elaborate on this PD? Could the voltage divide from the external I2C pullup and not be in compliance to voltage level requirements…

  • BQ28Z610-R1: Cell balancing accuracy

    Part Number: BQ28Z610-R1

    Hi team,

    I would like to know how much is the reading deviation (+/-%) of V_CELL? I understood the temperature is one of the factor, so that I want to know the total accuracy of V_CELL including ADC error.

    Regards,
    Kazuto

  • BQ28Z610-R1: Best battery option for this gauge IC

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ25883, , GPCCHEM

    Hello,

    I'm currently using the BQ25883 charger + BQ28Z610-R1 gauge, with 2x 18650 Li-ion batteries in 2S1P configuration, as my main circuit needs at least 6V. However, I had…

  • BQ28Z610: BQ28Z610 0.20 firmware

    Part Number: BQ28Z610

    Hello, I need to save a Golden Image with the BQ28Z610. I downloaded version 1.3.104 of the Battery Management Studio, but I have read that firmware version 0.20 is also required. My BQ28Z610 devices report version 0.17. Where can…

  • BQ28Z610-R1: RelativeStateOfCharge jumping from ~82% to 100%

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ25883, , GPCCHEM, BQ28Z610, BQSTUDIO

    Hello,

    Something is happening when charging/discharging the battery using the BQ25883 as charger + BQ28Z610-R1 as gauge:

    When using (discharging) the batteries…

  • BQ28Z610-R1: BQ28Z610-R1 I2C Standard Command Question

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ28Z610, BQ40Z50, BQ40Z80

    Hi Ti Team

    I made a smart battery using the BQ28Z610-R1. However, I receive strange data while communicating with the CPU. If you look at slucc81-57 page, there is Standard…

  • BQ28Z610-R1: Questions about the BQ28Z610-R1

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ25883, EV2400

    Hello,

    I'm having some issues with the BQ28Z610-R1, and to help solve it I got a few questions. For reference, this is my circuit, using the BQ25883 as charger and the BQ28Z610…

  • BQ28Z610-R1: When configuring for single cell, are VC1, VC2 tied together?

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ28Z610

    Oddly I can't find a diagram or text on this in the datasheet or technical reference.

    I'm hoping to replace a  bq27750 with a BQ28z610 and wondering if I need to change the PCB layout…

  • BQ28Z610: Does BQ28Z610 change to BQ28Z610-R1 shoud I change my rigister or other software

    Part Number: BQ28Z610

    Hi Expert

    My old design use BQ28Z610 ,and now we change to BQ28Z610-R1 . I have some consern about this new version.

    Does BQ28Z610 change to BQ28Z610-R1 shoud I change my rigister or other software lever change?

  • BQ28Z610: SLUUA65D - I2C Configuration register TO_STRETCH_EN and bqStudio

    Part Number: BQ28Z610
    Other Parts Discussed in Thread: BQSTUDIO, ,

    Hello, 

    because no replies yet at my previous post, I have tried to enable the TO_STRETCH_EN and to look what will happen....

    Now, it seems the problem with I2C bus errors (supposed errors…

  • BQ28Z610: 0.20 SREC file and others

    Part Number: BQ28Z610
    Other Parts Discussed in Thread: BQSTUDIO,

    The version 0.20 which has been present in the web site for more than 2 years suddenly has disappeared! 

    The reply to anyone is asking about it and why we should downgrade to 0.17 release…

  • BQ25883: BAT output vs. PACK input

    Part Number: BQ25883
    Other Parts Discussed in Thread: BQ28Z610-R1, BQ28Z610

    Hello,

    My circuit uses the BQ25883 for Charger, and the BQ28Z610-R1 for Gauge. This is my circuit:

    On the BQ25883, I have "Enable Charge" and the "Charge Voltage" set to 9.2V…

  • BQ28Z610-R1: product safety - short at VC1/VC2

    Part Number: BQ28Z610-R1

    Hello,

    we do have a product with a bq28z610-r1 for battery protection.

    At the moment we do a product-safety test and the following question did appear:

    - lets assume a first-error occurs and one of the marked parts (fuel gauge, 100nF…

  • BQ28Z610-R1: The detected device is not compatible with this application

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: EV2400, BQ28Z610, , BQSTUDIO

    Hello,

    I'm using the BQ28Z610DRZR-R1 on a board, and when I try to access it through Battery Management Studio using the EV2400, I get this message:

    When picking…

  • BQ28Z610-R1: FullChargeCapacity is jumping

    Part Number: BQ28Z610-R1

    Hi,

    I have charged and discharged few times and I saw some strange behaviors and hope you can help: 

    Charging from zero to full:

    * you can see that the charger is charging for >6200mAh 
    * when EoC is been detected and FCC is dropping…

  • BQ28Z610: I2C pull low to reset

    Part Number: BQ28Z610
    Other Parts Discussed in Thread: BQ25619,

    Hi, I am trying to file a related post to this one: https://e2e.ti.com/support/power-management/f/power-management-forum/803617/bq28z610-resetting-i2c-line-when-in-error-state

    I believe I…

  • BQ28Z610-R1: Linux driver

    Part Number: BQ28Z610-R1
    Other Parts Discussed in Thread: BQ28Z610

    Hello,

    Where can I get the latest Linux driver for BQ28Z610-R1?

    Regards,

    Kien