Other Parts Discussed in Thread: CSD18563Q5A
Our design has two LM5117 with same caracteristics:
Vin variable between 30Vdc and 42Vdc
Vout 12Vdc
Current Out Max 10A
With no load we have 12V output, but under any load we do not get
…Our design has two LM5117 with same caracteristics:
Vin variable between 30Vdc and 42Vdc
Vout 12Vdc
Current Out Max 10A
With no load we have 12V output, but under any load we do not get
…App Note "slua874" goes into calculating undershoot based on the compensation network (and even backs it up with a simulation!). Comparing the LM5117 compensation calculations to slua874 is NOT straight forward as the gain…
Hi Dear,
I am designing a DC-DC converter using LM5117. Can you please provide the LM5117EVAL layout for reference?
Thank you
I am trying to build an adjustable power supply, controlled from a potentiometer around the FB resistors, to provide between 10V and 33V up to 8A from a 48V input.
I have started…
Hello,
I am attempting to modify LM5117EVAL board to generate 20V output with 9A current capacity.
Using the LM5117 Quick Start Calculator, I found that the only R16 (357Ohm) should be changed…
Hello TI experts,
I am trying to design an adjustable constant current supply using the LM5117 chip that can source ~0-2A. Currently, I plan to modify the CC example in the datasheet:

Originally, I tried to replace the voltage divider…
Hi,
Good day.
Our customer has generated the design using webench. You can find it here: webench.ti.com/.../SDP.cgi. Their question is why the M1 and M2 are different transistors? What is the reason? Can they use same transistors here…
I used LM5117 to design two outputs, input voltage 25~40V, output1 is 12V/10A, output2 is 22V/4A, output 1 is ok, but output2 is less than 22V without load and is ok with load. They're…
Hello,
I designed controller and cannot get it to pass EMC. I have tried adding ferrits to input and output wires, changing CBoot, and adjusting values of…
Hi there,
I am designing a circuit for one of my projects with LM5117. My intend was to create a CC regulator with hiccup mode OVP which exists in the datasheet of LM5117.
And then i made a design with this configuration. The configuration…
When debugging LM5117, we found that the input voltage is lower than 45V, and the output is only 15V(issue). If we increase the voltage to 50V, the output is ok (normal output voltage is…
Hi Yew,
Is it stable at lower duty cycles, e.g. D < 50%? Please check compensation values with the quickstart calculator. By the way, the Cout of 660uF is very high given the high Vout in this design. Also, the VCC cap should be 1uF and boot cap can…