I have a need for a high voltage (~1000V) bias (almost zero current) supply used in detecting ionization. I've looked at a design from Maxim, but it requires a custom toroid coil which is causing me headaches.
The requirement is to use an existing 12V (or similar low voltage) supply to generate a postive high voltage. This is applied to a plate that will force alpha particles away - towards ground potential. There is no specification for the ripple as it could be a couple volts and not have an effect on the outcome.
I was just wondering what the E2E community might recommend.