This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMZ14201H: Generate Positive and Negative power rails using LMZ14201H

Intellectual 575 points

Replies: 1

Views: 384

Part Number: LMZ14201H

Hi, I found in AN-2027 that LMZ14201 can be used to generate negative power rails. Can I use two LMZ14201H to generate +10V and -10V powers from 5V supply? The reason I want to use LMZ14201 power module is that it has small pin counts and do not need any additional inductors. The power requirements is +10V, 200mA and -10V 200mA, so I need some quick solutions to my problem. BTW, I do not need any enable or UVLO features, so is it ok to tie EN to VIN?
  • Hello Byliu,

    Yes, you can use the LMZ14201H with the Application note. The "H" and the non"H" devices are pin-to-pin compatible.

    It is OK to tie EN to VIN.

    Cheers,
    Denislav

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.