This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS40303: SS PIN function queries.

Expert 2135 points

Replies: 3

Views: 181

Part Number: TPS40303

Hi,

    Is TPS40303's SS pin have tracking function like LM25145 or TPS54824?

   Or the IC have the tracking function?

 

thanks.

  • Hi,

    Let me check with the application engineer that might handle this product.

    Thanks
    -Arief
  • Wu,

    Since the EN/SS pin are combined together it will be tricky to use as a classical tracking function. There is also an offset involved of 0.8V which makes it not useful for a track function.

    Regards,

    Mathew

  • In reply to Arief Hernadi:

    Hi Arief,
    Any feedback for AE?
    thanks.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.