This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

UCC28780EVM-002: UCC28780 HV MOSFET damage issue

Genius 3200 points

Replies: 2

Views: 766

Part Number: UCC28780

Dear,


our client reference design TIDA-01622  relayout new power board ,But find the IC HV start up 600v MOSFET was damage and output cannot load. 

ACF 65W Type-C.pdf

HV damage part: infineon BSS126

DC147V output 20V Vsw pluse 4

Channl 1 FB  Channl2 VSW

but If yellow highlight CS pin change connect to GND, the power board was can work.

If any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence.

 

  • Dear Lawrence,

    Thanks for promoting TI's solution to your customer.
    It might related the layout issue, cause too high di/dt on the HV MOSFET.
    I will discuss with senior AE and get back to you soon

    Best Regards
    Kevin
  • In reply to Kuan Wei Chen (Kevin Chen):

    Dear Lawrence,

    Sorry for take such a long time to figure out your issue.
    Can you help me to change RP38 from 4.7 to 5000ohm?
    It might be high side isolator mis-turn on your high side GaN, which cause high di/dt to damage your HV MOSFET's Vgs.

    I check the UCC28780EVM002 design.
    They put 4.99kohm to mitigate the mis-turn on issue on high side GaN

    I hope this can fix it.

    Best Regards
    Kevin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.