This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Suitable IC Package for Light Dimer use for controlling Street light through Wireless Light Sensor

Prodigy 150 points

Replies: 5

Views: 282

I need to use some light dimer IC package with the suggested circuit which will be controlled by the wireless Light sensor using creating the mesh network for a smart street light system.

Any pieces of advice on this will be much help.

  • Hello Robson Jhon,
    Are you looking for the dimming circuit or the wireless portion?
    If the dimming control is needed please provide Input voltage range and the lighting load (voltage and current).


    Best Regards,

    Ed Walker

  • In reply to EdWalker:

    Hello Robson Jhon,
    This reference design you may find interesting.
    100W Dimmable DC-DC LED Driver with Daylight Harvesting and Wireless Connectivity Reference Design

    The TIDA-01095 TI design is a tested DC-DC LED driver subsystem for high power, high efficiency dimmable LED luminaires. It is built-on a wireless SoC platform which can enable intensity adjustment through analog, PWM dimming and control using any BLE smart device or ZiBee. High Bay and Low bay LED lighting luminaires are replacing the fluorescent and HID lights as they cut energy consumption in half and nearly eliminate maintenance costs. Daylight harvesting using the dimming feature combined with ambient light sensor, can provide up-to additional 50% energy savings depending on the application. TI design TIDA-01095 provides high efficiency DC-DC conversion, allows dimming, daylight harvesting and enables wireless connected lighting control.

    www.ti.com/.../TIDA-01095


    Best Regards,

    Ed Walker

  • In reply to EdWalker:

    Hi EdWalker

    Thanks a lot for your reply actually we want to use around 28 LED street lamps which are connected with every home in a row with 50 m Far  distance  from each other and We are connecting to the  power supply individually as per mentioned below specifications

    ModelLED Street Lights LU1
    Power Efficiency 85%
    Working Voltage 24VDC
    LED Consumption 28 Watt
    Power Supply Consumption 7 Watt

    And major Point is we need to control the dimming of LED lamps as per the Wireless Light sensor data through single circuit

    Also, at the same time we want to recharge the 24v DC battery used individually should get charged from the circuit (which should be connected with all the 24v Battery)

    - After every 50% of consumption, the charging criteria will work automatically.

    - The major issue is the wiring problem where I actually need the suggestion to avoid voltage drop in my circuit.

    Any suggestions on this will be much useful.

  • In reply to Robson Jhon:

    You cannot modify Ohm’s Law, so resistive drop will always be present.
    1. PoE, Power Over Ethernet, raised the working voltage above 48V to 57V so less current is drawn, thus less loss.

    2. Streetlights could be on a timeshare basis where only a certain number at a time pull current from the 48V. Don’t try to charge them all at once.

    3. One great option to help with long loop voltage drop is to go solar.

    Here is a seminar paper on the subject.
                   ( http://www.ti.com/ww/en/power_supply_design_seminars/index.html )

    My vote here is the digital C2000 method, much more versatility.

     

    Designing a Solar-Cell-Driven LED Outdoor Lighting System
    White Paper        http://www.ti.com/lit/slup267Presentations   http://www.ti.com/lit/slup260

    A solar-powered LED light is an obvious application given the growing interest in “green” systems. This topic will use a medium-power solution to illustrate the many considerations of designing a complete system, including the unique demands of both the solar array and the LED lamps, and integrating these with a storage battery, charger, and control circuitry. Both analog and digital power-control solutions will be proposed and compared on the basis of functionality, complexity, and cost.

      

    Reference design:
    Solar Street Light with Integrated MPPT Charger Reference Design

    This design is a 12A Maximum Power Point Tracking (MPPT) solar charge controller with a 700mA LED driver. It is targeted for low power solar charger and LED driver solutions such as solar street lights. This design is capable of charging 12V batteries with up to 10A output current from 12V panels. However, it can be easily adapted to 24V systems by just changing the MOSFETs to 60V rated parts. Also, the design can drive up to 15 LEDs in series with 700mA of current. It is possible to adapt the design for LED currents up to 1.1A with minimum change in hardware. TI provides a complete solar inverting system for low power loads. Additionally this design takes real world considerations in to account, such as reverse battery protection, built-in battery charge profile for 12V Pb-acid batteries, and a highly efficient design. Together these provide new market entrants and faster time to market for their design.

     

     

    TI has application suggestions in our APPLICATIONS area.

    TI Home Applications Industrial Lighting > LED Luminaire > Outdoor Lighting

    http://www.ti.com/solution/lighting_streetlight_arealight_highbay_midbay

    Outdoor LED lighting IC solutions from TI demonstrate innovative solutions for streetlight, area lighting, high bay and mid bay lighting systems. Reference designs, system block diagrams (SBDs) and other technical resources showcase TI’s AC/DC, DC/DC, LED driver, power management, and wireless connectivity portfolios.

     

    Blue boxes indicate TI solutions, click to show details on the right side of the page.

    Clicking a box turns it red.


    Best Regards,

    Ed Walker

  • In reply to EdWalker:

    Hello Robson,

    I haven't heard back from you in a few days so I'm going to close this thread. If you have additional comments or questions, just reply and the thread will reopen.


    Best Regards,

    Ed Walker

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.