This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMG3410R070: LMG3410-Rated Design

Intellectual 980 points

Replies: 1

Views: 184

Part Number: LMG3410R070

Hi,

We want to use 6 X LMG3410. Operating at 480VDC. Is there any evaluation module or reference design that would allow us to do that?

·       The thermal design of TIDA-00915 allows us to work only up to 200V

·       The EVM LMG3410-HB-EVM seem to have a mother board that takes only one of these evaluation modules.

Do you have another motherboard that would allow us to use three of these EVMs?

Regards

Sam

  • Hello,

    This TIDA-00915 is able to support voltage up to 450V. We do not have further info for 480V operation but it does not mean it cannot. This really depends on the on-board component voltage rating. There are no other motherboards that can support three EVMs together. Hope it helps.

    Thanks and regards,

    Lixing

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.