This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Is it possible to boost 12 V to 1000 V? The 12 V input is coming from a battery.

Prodigy 125 points

Replies: 6

Views: 145

I have an application where in I require 1000 V DC from a 12 V battery. Is there any fly back or multistage boost converter available to achieve this? 

  • Hi Getssy,

    Thanks for reaching out with your question.

    What is the output current of the 1000V rail? And is isolation required in the design?

    Thanks,

    Garrett
  • In reply to Garrett Roecker:

    Dear Garrett,

    Thank you for your kind reply. Isolation is not mandatory requirement for the circuit. Its a low current application ( if possible a maximum of 1 A or so, if not mA should also be fine).
  • In reply to Getssy prathiba:

    Hi Getssy,

    Before we can come up with a solution the output current needs to be defined. If the output current is 1A then this will be a difficult design.

    Thanks,

    Garrett
  • In reply to Garrett Roecker:

    Dear Garrett,

    Could you please let me know what can be the maximum current possible with a standard design?

    Best Regards, 
    Getssy  

  • In reply to Getssy prathiba:

    Hi Getssy,

    Assuming the output is 1A the average input current is going to be ~83A. To find reasonably sized components this would need to be a multi-phase design. Possibly 3 phases would work.

    Can you please tell me what the application is? This is not a common application specification.

    Thanks

    Garrett
  • In reply to Getssy prathiba:

    Hello Getssy,

    With such a high boost ratio there are typically several stages used.
    Boost + charge pumps, flyback with stacked windings, multipled SEPIC, are some of the topologies used.
    Output currents  for a high boost ratio are usually in the 10's of mA range, or lower.

    Please see http://www.ti.com/tool/PMP30104  as an example.
    A SEPIC converter is used to charge a load capacitor (up to 15000uF) up to 400V/420V (selectable).
    The input voltage range is 15V +/-10% and the constant output charging current 80mA.
    The multiplied SEPIC topology has several advantages compared to Boost + charge pump mainly thanks to reduce peak and RMS currents in the multiplier of the SEPIC.

    http://www.ti.com/tool/PMP20212 
    This low current boost converter implements a voltage doubler which allows a high input-to-output boost ratio.
    This design is low cost and requires an area of 16mm x 27mm.
    More stages of voltage doubler can be added to increase Vout.

    http://www.ti.com/tool/PMP20183 
    This boost converter implements a voltage tripler which allows a high input-to-output boost ratio.
    The design is low cost and requires an area of less than 25mm x 25mm.

    Finally, this PMP design is not public yet, however I will forward the details.
    PMP20899 is a 6-8.4Vin and makes 1500Vout at 20mA.
    It is a stacked flyback approach.
    Schematic, BoM, Test Report are attached.

    PMP20899na(001)_Sch.PDFPMP20899na(001)_TI-BOM.pdfPMP20899 TestReport.pdf

    There is not an example of 12V to 1000V in our archives, however the 4 examples above show the possibilities.


    Best Regards,

    Ed Walker
    Texas Instruments 
    Online Support - Systems & Tools

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.