This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 82
Part Number: TPS62356
Hi,
I need a DC/DC with I2C to control the output current .
But TPS62356 current is too small I need 3A like NCP6343.
Could you help?
Hello,
I suggest you take a look at these two TI products, that might fit more your application : TPS65263 / TPS65263-Q1
They share some common features. To help you better, can you share what would be your application?
Thank you for reaching out to us!
Regards,
Dorian
________________________________
TPS62147 – New 17Vin, 2A buck with forced-PWM option for low output ripple.1% accuracy over temperature, 0.8V to 12Vout, pin-compatible to 4A (TPS62136), for industrial applications.
In reply to Dorian Brillet de Cande:
In reply to user4215035:
Sure! Then the TPS6236x family is a better fit to your application.
Can you have a look at these? as well as the TPS62366x?
Thank you.