This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM2575: Can LM2575 be used to replace Renesas, M51995?

Guru 10840 points

Replies: 4

Views: 114

Part Number: LM2575

 Hello guys,

 One of my customers is looking for any TI device can replace Renesas, M51995 because the device is EOL soon.

・M51995
https://datasheet.octopart.com/M51995AFP%23CF0J-Renesas-datasheet-136336.pdf

 I think LM2575 or UC2524A could replace the Renesas device. Is my understanding correct? If do you have any recommended device, could you please let me know?

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.  

  • Yes, if you need the same package then you can use the LM2575.
    If you can change the package, then we have plenty of newer device available, surface mount available.

    Thanks
  • In reply to Arief Hernadi:

    Hello Arief,

    Thank you very much for your reply.

    The customer needs surface mount packege.
    Could you please tell me any device which can be used for Renesas, M51995 replacing?

    Thank you again and best regards,
    Kazuya Nakai.
  • In reply to Kazuya Nakai54:

    You might want to look at LM43601 or the LM2675 or the LM22675
  • In reply to Frank De Stasi:

    Hello Frank,

    Thank you for your reply. I will introduce thoese device to the customer.

    Best regards,
    Kazuya Nakai.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.