This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Isolated DCDC converter, 24Vin, 24Vout

Genius 9485 points

Replies: 1

Views: 50

Hello,

We are looking for 24Vin 24Vout isolated DCDC converter. Is there any device to match this spec?

In my search, DCV012415D or DCP012415DB, 24Vin +/- 15V module is the most closest. Should we use +30V output + LDO for making 24V in this case?

Best regards,

Toshihiro Watanabe

  • Hi Watanabe-san,

    Is an isolated DC/DC a requirement? The power module portfolio does not have any solution for an isolated 24Vout device. However, for non-isolated DC/DC buck power module, there is the LMZ14201H in a leaded package that allows a 42Vin_max to 24Vout_max solution. Would this be a proper alternative to your application?

    Regards,
    Jimmy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.