This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS61175: Can flyback usage support an isolated 48V output?

Intellectual 830 points

Replies: 8

Views: 157

Part Number: TPS61175

Team

My customer is looking for a 14V input, isolated 48V output (max 15.4W) boost converter.

There is TPS61175PWPR (~ 18V input, ~ 40V output) and it was written that the flyback can be supported

in datasheet. 

Even if it is IC of rated output 40V, if it is flyback method,

is it possible to make 48V output on the secondary side of the transformer with TPS61175?

Thanks

Best regards,

Shidara

  • Hi K.

    The engineering supporting this device is current ooo on holidays until after May 3rd. I think it is possible but the max voltage stress on the SW should be less than 40V. You need to consider the min input voltage to select the max duty cycle and transformer turns ratio, and assess the max SW stress under the max input voltage. Please refer to the tool at the following link to help you.

    www.ti.com/.../flybuck-flyback-design-calc


    Thanks,
    Youhao
  • Hi-Shidara,

    Youhao is right. what is the input voltage range?

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    Hi Helen-san

    Thank you very much for the advice.

    Let me double check the input condition.

    Thanks

    Best regards,

    Shidara

  • In reply to K.Shidara:

    Dear Sir,
    Any feedback on the input condition?

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    Hi Helen

    Thanks for your reminder.

    Input condition is 14V±2V.

    Thanks

    Best regards,

    Shidara

  • In reply to K.Shidara:

    Hi Shidara,
    The Vin variation range is not big. So a flyback topology is OK for this design. you can set Np:Ns=2:5 to achieve the target. And you can add a RCD snubber at the primary side to supress the spike.

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    Hi Helen-san

    Thank you so much for your advice.

    Understood.

    Thanks

    Best regards,

    Shidara

  • In reply to K.Shidara:

    You're welcome! Good Luck!

    Best Regards,
    Helen

    Boost DC/DC Solution

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.