• TI Thinks Resolved

TPS61175: Can flyback usage support an isolated 48V output?

Prodigy 590 points

Replies: 6

Views: 114

Part Number: TPS61175

Team

My customer is looking for a 14V input, isolated 48V output (max 15.4W) boost converter.

There is TPS61175PWPR (~ 18V input, ~ 40V output) and it was written that the flyback can be supported

in datasheet. 

Even if it is IC of rated output 40V, if it is flyback method,

is it possible to make 48V output on the secondary side of the transformer with TPS61175?

Thanks

Best regards,

Shidara